cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H733 data cache initialization issue

amirshn
Associate III

Hello,

I am using a STM32H733VGT on a custom design board. On a fresh project in CubeMX, I tried to activate data cache but the autogenerated code crashes at  SCB_EnableDCache(); . (nothing has been activated on the CubeMX, just the external crystal and debugging port)

i tried enabling or disabling MPU as well, same results.

I need data cache for activating ethernet.

 

Any help would be highly appreciated.

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

I didn't find that exact device STM32H733VGT but tested your ioc file on NUCLEO-H723ZI board (STM32H723ZI) and I didn't reproduce the behavior.

Don't step into SCB_EnableICache() and SCB_EnableDCache().

If you put a break point on HAL_Init() and run, do you reach it? 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

9 REPLIES 9
mƎALLEm
ST Employee

Hello,

Are you sure you've generated a project for STM32H733 and not another MCU device?

Is that possible to share your ioc file?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi 
I think so , here is my ioc file:

Thanks

Could you please replace the MPU config like the following?:

void MPU_Config(void)
{
  MPU_Region_InitTypeDef MPU_InitStruct = {0};

  /* Disables the MPU */
  HAL_MPU_Disable();

  /** Initializes and configures the Region and the memory to be protected
  */
  MPU_InitStruct.Enable = MPU_REGION_ENABLE;
  MPU_InitStruct.Number = MPU_REGION_NUMBER0;
  MPU_InitStruct.BaseAddress = 0x0;
  MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
  MPU_InitStruct.SubRegionDisable = 0x87;
  MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
  MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
  MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
  MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
  MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
  MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

  HAL_MPU_ConfigRegion(&MPU_InitStruct);
  /* Enables the MPU */
  HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi,

tried that, no difference, it stuck in the activation function of data cache.

Would you explain me what are suspicious about?

 

Thanks a lot for you help

I don't see an issue for the moment and I don't have that device for the moment to test.. I'll get back to you when I test it.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thanks a lot for that.

BTW, is it necessary to enable Dcache to activate ethernet for this MCU?

The cache is enabled to enhance the performance of all the application, not only for ethernet.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

Hello,

I didn't find that exact device STM32H733VGT but tested your ioc file on NUCLEO-H723ZI board (STM32H723ZI) and I didn't reproduce the behavior.

Don't step into SCB_EnableICache() and SCB_EnableDCache().

If you put a break point on HAL_Init() and run, do you reach it? 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi,

yeah, that's the case, unexpectedly if I put a breakpoint after these two (SCB_EnableICache() and SCB_EnableDCache()) , I'll reach HAL_Init(). (I just figured this out).

Could you tell me why is it behaving like this?

 

Thanks a lot for your help.