2024-02-10 10:45 PM - edited 2024-02-10 11:23 PM
Greetings,
I have a problem with LWIP when the D-Cache is enabled.
My test program:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* USER CODE BEGIN Boot_Mode_Sequence_0 */
int32_t timeout;
/* USER CODE END Boot_Mode_Sequence_0 */
/* Enable the CPU Cache */
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
/* USER CODE BEGIN Boot_Mode_Sequence_1 */
/* Wait until CPU2 boots and enters in stop mode or timeout*/
timeout = 0xFFFF;
while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0));
if ( timeout < 0 )
{
Error_Handler();
}
/* USER CODE END Boot_Mode_Sequence_1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* Configure the peripherals common clocks */
PeriphCommonClock_Config();
/* USER CODE BEGIN Boot_Mode_Sequence_2 */
/* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of HSEM notification */
/*HW semaphore Clock enable*/
__HAL_RCC_HSEM_CLK_ENABLE();
/*Take HSEM */
HAL_HSEM_FastTake(HSEM_ID_0);
/*Release HSEM in order to notify the CPU2(CM4)*/
HAL_HSEM_Release(HSEM_ID_0,0);
/* wait until CPU2 wakes up from stop mode */
timeout = 0xFFFF;
while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0));
if ( timeout < 0 )
{
Error_Handler();
}
/* USER CODE END Boot_Mode_Sequence_2 */
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_LWIP_Init();
MX_RAMECC_Init();
/* USER CODE BEGIN 2 */
printf("H747 - M7 - " __DATE__ " " __TIME__ "\r\n");
struct udp_pcb *pcb;
err_t err;
struct pbuf *p;
pcb = udp_new();
if (!pcb)
{
printf("udp_new() failed\r\n");
Error_Handler();
}
ip_addr_t dest_ip;
IP4_ADDR(&dest_ip, 10, 97, 0, 1);
const u16_t dest_port = 1997;
if ((err = udp_connect(pcb, &dest_ip, dest_port)) != ERR_OK)
{
printf("udp_connect() failed\r\n");
Error_Handler();
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
MX_LWIP_Process();
p = pbuf_alloc(PBUF_RAW_TX, 3, PBUF_RAM);
if (!p)
{
printf("pbuf_alloc() failed\r\n");
Error_Handler();
}
pbuf_take(p, (char*)"123", 3);
if (udp_send(pcb, p) != ERR_OK)
{
printf("udp_send() failed\r\n");
//Error_Handler();
}
pbuf_free(p);
}
/* USER CODE END 3 */
}
it's working fine when comment out the SCB_EnableDCache().
Log when D-Cache disabled:
pbuf_alloced_custom(length=0)
ethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:ff
pbuf_remove_header: old 0x24004048 new 0x24004056 (14)
ip_input: iphdr->dest 0xffffff0a netif->ip_addr 0x200610a (0xffff0a, 0x610a, 0xff000000)
ip4_input: packet not for us.
pbuf_free(0x24004028)
pbuf_free: deallocating 0x24004028
pbuf_alloced_custom(length=0)
ethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:ff
pbuf_remove_header: old 0x24003a28 new 0x24003a36 (14)
etharp_update_arp_entry: 10.97.0.1 - e0:d5:5e:31:03:c3
etharp_find_entry: found matching entry 0
etharp_update_arp_entry: updating stable entry 0
etharp_input: incoming ARP request
etharp_input: ARP request was not for us.
pbuf_free(0x24003a08)
pbuf_free: deallocating 0x24003a08
pbuf_alloced_custom(length=0)
ethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:ff
pbuf_remove_header: old 0x24003408 new 0x24003416 (14)
ip_input: iphdr->dest 0xffffff0a netif->ip_addr 0x200610a (0xffff0a, 0x610a, 0xff000000)
ip4_input: packet not for us.
pbuf_free(0x240033e8)
pbuf_free: deallocating 0x240033e8
sct calling h=ip_reass_tmr t=975 arg=0x801af6c
tcpip: ip_reass_tmr()
sys_timeout: 0x240055ac abs_time=22308 handler=ip_reass_tmr arg=0x801af6c
sct calling h=etharp_tmr t=974 arg=0x801af78
tcpip: etharp_tmr()
etharp_timer
sys_timeout: 0x24005598 abs_time=22321 handler=etharp_tmr arg=0x801af78
pbuf_alloc(length=3)
pbuf_alloc(length=3) == 0x30044008
udp_send
pbuf_add_header: failed as 0x30044010 < 0x30044018 (not enough space for new header size)
pbuf_alloc(length=8)
pbuf_alloc(length=8) == 0x30044024
pbuf_chain: 0x30044024 references 0x30044008
udp_send: added header pbuf 0x30044024 before given pbuf 0x30044008
udp_send: sending datagram of length 11
udp_send: UDP packet length 11
udp_send: UDP checksum 0x0000
udp_send: ip_output_if (,,,,0x11,)
pbuf_add_header: old 0x30044058 new 0x30044044 (20)
ip4_output_if: st0
IP header:
+-------------------------------+
| 4 | 5 | 0x00 | 31 | (v, hl, tos, len)
+-------------------------------+
| 16 |000| 0 | (id, flags, offset)
+-------------------------------+
| 255 | 17 | 0x0000 | (ttl, proto, chksum)
+-------------------------------+
| 10 | 97 | 0 | 2 | (src)
+-------------------------------+
| 10 | 97 | 0 | 1 | (dest)
+-------------------------------+
ip4_output_if: call netif->output()
pbuf_add_header: old 0x30044044 new 0x30044036 (14)
ethernet_output: sending packet 0x30044024
Prepare bytes: E0h D5h 5Eh 31h
pbuf_free(0x30044024)
pbuf_free: deallocating 0x30044024
pbuf_free: 0x30044008 has ref 1, ending here.
pbuf_free(0x30044008)
pbuf_free: deallocating 0x30044008
Log when D-Cache enabled:
sct calling h=ip_reass_tmr t=358 arg=0x801afec
tcpip: ip_reass_tmr()
sys_timeout: 0x240055ac abs_time=26418 handler=ip_reass_tmr arg=0x801afec
sct calling h=etharp_tmr t=328 arg=0x801aff8
tcpip: etharp_tmr()
etharp_timer
etharp_timer: expired pending entry 0.
etharp_free_entry: freeing entry 0, packet queue 0x30044024.
pbuf_free(0x30044024)
pbuf_free: deallocating 0x30044024
pbuf_free: deallocating 0x30044008
sys_timeout: 0x24005598 abs_time=26460 handler=etharp_tmr arg=0x801aff8
pbuf_alloc(length=3)
pbuf_alloc(length=3) == 0x30044008
udp_send
pbuf_add_header: failed as 0x30044010 < 0x30044018 (not enough space for new header size)
pbuf_alloc(length=8)
pbuf_alloc(length=8) == 0x30044024
pbuf_chain: 0x30044024 references 0x30044008
udp_send: added header pbuf 0x30044024 before given pbuf 0x30044008
udp_send: sending datagram of length 11
udp_send: UDP packet length 11
udp_send: UDP checksum 0x0000
udp_send: ip_output_if (,,,,0x11,)
pbuf_add_header: old 0x30044058 new 0x30044044 (20)
ip4_output_if: st0
IP header:
+-------------------------------+
| 4 | 5 | 0x00 | 31 | (v, hl, tos, len)
+-------------------------------+
| 20 |000| 0 | (id, flags, offset)
+-------------------------------+
| 255 | 17 | 0x0000 | (ttl, proto, chksum)
+-------------------------------+
| 10 | 97 | 0 | 2 | (src)
+-------------------------------+
| 10 | 97 | 0 | 1 | (dest)
+-------------------------------+
ip4_output_if: call netif->output()
etharp_find_entry: found empty entry 0
etharp_find_entry: selecting empty entry 0
etharp_request: sending ARP request.
pbuf_alloc(length=28)
pbuf_alloc(length=28) == 0x30044068
etharp_raw: sending raw ARP packet.
pbuf_add_header: old 0x30044088 new 0x3004407a (14)
ethernet_output: sending packet 0x30044068
Prepare bytes: FFh FFh FFh FFh
ETH_ERROR_BUSY
pbuf_free(0x30044068)
pbuf_free: deallocating 0x30044068
etharp_query: queued packet 0x30044024 on ARP entry 0
pbuf_free(0x30044024)
pbuf_free: 0x30044024 has ref 1, ending here.
pbuf_free(0x30044008)
pbuf_free: 0x30044008 has ref 1, ending here.
Has anyone encountered this problem?
Solved! Go to Solution.
2024-02-12 02:26 AM
Hello @hzoli and welcome to the Community
I recommend you to take a look at How to create project for STM32H7 with Ethernet an... - STMicroelectronics Community and at STM32H747_Disco_M7_ETH example may help you. The Dcache is enabled in these examples.
Also, I advise you to check the MPU configuration.
Pease note that, if the cache is enabled, it is requires to follow this order: configure MPU firstly, then enable cache.
/* MPU Configuration--------------------------------------------------------*/
MPU_Config();
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-12 02:26 AM
Hello @hzoli and welcome to the Community
I recommend you to take a look at How to create project for STM32H7 with Ethernet an... - STMicroelectronics Community and at STM32H747_Disco_M7_ETH example may help you. The Dcache is enabled in these examples.
Also, I advise you to check the MPU configuration.
Pease note that, if the cache is enabled, it is requires to follow this order: configure MPU firstly, then enable cache.
/* MPU Configuration--------------------------------------------------------*/
MPU_Config();
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-12 03:50 AM - edited 2024-02-12 03:53 AM
Hello,
You need to disable the cache for Rx and Tx ETH descriptors and LWIP heap using MPU. You have a data coherency issue:
So as said by @KDJEM.1 , refer to the link https://community.st.com/t5/stm32-mcus/how-to-create-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308
Also please refer to the AN4839 "Level 1 cache on STM32F7 Series and STM32H7 Series" for cache usage and mistakes to avoid.
2024-02-12 10:41 PM - edited 2024-02-12 10:41 PM
Thank you all! After I configured the MPU, the LWIP heap address and modified the linker script, now working perfectly.
@SofLit Thank you for the tip and the documentation link about "Level 1 cache".