NUCLEO-H755 - ETH configured (Non-RTOS) but LWIP remains grayed out
- 3 replies
- 1954 views
Hi STM32 friends,
I'm about to learn something new, because I hit a problem with STM32CubeMX 6.11.1 (newest)
I have used Ethernet on several M7 platforms, not always without a bit of struggling.
However, this time after configuring ETH, LWIP remains grayed out.
I'm using a NUCLEO-H755ZI-Q, which has an M4 and M7 core. I use the M7 core for ETH.
There are no warnings at the ETH configuration, except:
"The ETH can work only when RAM is pointing at 0x24000000"
So I modified the First Tx Descripter Address to 0x24000200, and First Rx Descripter Address 0x24000000.
(I guess they were wrong at first: 0x30000200 and 0x30000000)
The warning remains nevertheless.
The problem is LWIP remains grayed out.
The M7 DCache is enabled (as well as the ICache).
I configured the MPU:
Region 0:
Address: 0x24000200
Size: 16KB
SubRegion: 0x0
TEX: level 1
Access: ALL ACCESS PERMITTED
Instruction: ENABLE
Shareability: ENABLE
Cacheability: DISABLE
Bufferable: DISABLE
Region 1:
Address: 0x24000000
Size: 256B
SubRegion: 0x0
TEX: level 0
Access: ALL ACCESS PERMITTED
Instruction: ENABLE
Shareability: ENABLE
Cacheability: DISABLE
Bufferable: ENABLE
I'm not using RTOS here (as in previous projects, where it worked).
LWIP reports:
Status: Not available: Active only if: ETH IP configured / FREERTOS is enables when MBEDTLS is enabled.
I understand from this that only having ETH IP configured should be sufficient, as I don't use MBEDTLS.
ETH IP is configured. I don't use FREERTOS and MBEDTLS.
What can cause this problem that LWIP remains grayed out?
I attached my ios file, to make playing around easy.
I hope somebody has seen this or knows the solution.
Thank you very much for helping out!
Note: I didn't find the "ETH" label to add for this post.