2024-10-02 06:28 AM
I am trying to run a code that's built using STM32L1x_Peripheral Libs for STM32L151CBUxA MCU.
As soon as I run the SystemInit function inside the ResetHandler I am hitting a Hardfault, so I investigated the SystemInit function.
Once the Vector Table relocation function is executed in it a HardFault is caused. I am unsure how to debug or resolve this.
Please help me debug the code.
2024-10-02 06:48 AM
Hello @gkowshik ,
Could you please provide your source code file or direct me to the example you are currently working on in order to investigate the issue on my side ?
With regards,
2024-10-02 07:02 AM - edited 2024-10-02 07:04 AM
Hi @SHs ,
I am using a custom code, I am porting nRF8001 BLE library, I can attach the zip of my code here. I believe the hardfault is coming from the SystemInit function especially.
I did some digging into the hard fault and found the obvious instruction that's causing it i.e., the nop instruction right after the SystemInit function is executed (shown in the picture in previous reply). I need expert help to root cause it better.
Thanks