2024-10-06 11:15 PM - last edited on 2024-10-07 01:24 AM by Andrew Neil
I executed "Clock Example" on stm32H747I DISCO. I found that after two minutes of execution, the analog clock was about 15 seconds slower. After 53 minutes of execution, it was about 5 minutes slower, and it will become slower and slower. I did not add any The program code is in the M7 core. The way I compare is to enable RTC and uart in the M4 core, use the HAL_RTC_GetTime() function to read out the rtc time every second, and print it out through the uart. My question is, If the analog clock really slows down, is there any way I can correct it without users noticing?
2024-10-07 12:53 AM - edited 2024-10-07 12:58 AM
Hello @Kenwang ,
Did you test with smooth calibration ?
Check the calibration Settings (RTC_CALR register setting).
Are you using an external crystal or with an external clock?
Please check the section "Verifying the RTC calibration" in RM0399.
2024-10-07 01:08 AM
I have compared the time on the computer, it is really slow, and if you stare at the screen, its second hand will sometimes stop for a long time.
2024-10-07 01:28 AM
@Kenwang wrote:it will become slower and slower.
Is it actually slowing down, or is it just running at a constant slow rate?
Have you checked the accuracy of the timebase source for this analogue clock?
2024-10-07 01:37 AM
Hello @Kenwang ,
Could you please tell which "Clock Example" you are referring to?