cancel
Showing results for 
Search instead for 
Did you mean: 

Target Voltage Detection Fail Issue

BRobe.3
Associate III

Hello,

I got a stlm32 disco board. I cannot Flash.

So,I used STM32 ST-LINK UTILITY. Any connection fail even under reset. This one show Target Voltage Detection Fail. The board is powered by the USB CN2 Connector. The measurment on the CN4 Connector shows 3,3 v between 1 and 3 pins.( which seems normal)

Could this be a software issue ?

Best regards,

10 REPLIES 10
OB
Associate II

Hi BRobe.3. I'm currently experiencing the same issue. Did you find a solution?