cancel
Showing results for 
Search instead for 
Did you mean: 

SWO Viewer in ST-LINK Utility

Vignesh_V
Associate II

Hi Friends,

 I need Yours Help. I have  working on  STM32F407VET6  development board  and  I have to write on simple code like count the values. I want to see the data in SWO (Serial Wire Viewer).But using STM32CUBEIDE to flash the code to my code is not Done . Because, My board  is not support to flash the code by using STM32CUBEIDE.So,I have using ST-LINK Utility to flash the code to my board. But SWO is correctly enabled but unfortunately count value is not print in the SWO viewer. So, how to I have the data in SWO Viewer. I have to attach the my software screenshot and source code for your reference that boxed line only I have  add to see the count values. Thanks in  advance for yours Guidance .

 

22 REPLIES 22

I talking with stm32 based blue pill board like STM32F103C8 (if this type Blue Pill board is Industrial Standard and another question is this blue pill board is manufactured by STmicroelectronics )

https://stm32-base.org/boards/STM32F103C8T6-Blue-Pill.html 

Can You have to give any tutorials complete course regarding STM32 in video format for your suggestion?

Example: To access the all peripherals step by step procedure using HAL Drivers.

 


@AScha.3 wrote:
But i would recommend to buy (from his source in India) a STM board like this:

Yes, the "Discovery" and "Nucleo" are ST's low-cost development boards.

  • "Nucleo" tends to be just the STM32 (and ST-Link) with no extra bells or whistles (just a LED and button) - so lowest cost;
  • "Discovery" adds some more extras: in this case, gyroscope, e-compass, digital microphone, audio DAC with integrated class‑D speaker driver - so likely more expensive:
    https://www.st.com/en/evaluation-tools/32f411ediscovery.html

 

Depends if those "extras" are valuable to you - when they're not, I find they get in the way.

 

 

 

Again, it is 98% certain that any  "Blue Pill"  will not have a genuine STM32 on it.

 


@Vignesh_V wrote:

 is this blue pill board is manufactured by STmicroelectronics


No.

 


@Vignesh_V wrote:

Can You have to give any tutorials complete course regarding STM32 in video format


AndrewNeil_0-1717592439820.png

 

See also the STM32 MCU Developer Zone:

https://www.st.com/content/st_com/en/stm32-mcu-developer-zone.html 

And ST's YouTube Channel: 

https://www.youtube.com/channel/UCjnmZw3h4XnpK3e5D2jvIGA