2022-10-14 03:31 AM
Hi,
I designed and tried to use my custom board based on STM32F030R8T6 MCU. But the problem started from beginning.
For MCU Flashing I used STM32CubeProgrammer and ST-LINK V2 (STM8 & STM32) dongle.
First of all I was trying to connect the board and I've got "No STM32 target found!" Error.
Second, after NRST Reset button was pressed (this option I considered on my board) and STM32CubeProgrammer Connect pressing, releasing NRST Reset button I succeeded to connect the MCU.
After that, I've erased the chip completely and tried to flash my bin file. But I've got errors reg., Connection to device is lost.
There are two errors in the log list: "Unable to read device id from ROM table" and "Unable to get core ID".
I thought it was problem with board soldering and used another board. But the same issue was with second board as well.
Is there any solution how to rectify the above problem? Did anybody has such issue on custom boards?
Thanks in advance.
Solved! Go to Solution.
2022-10-15 09:06 AM
Ok then from your first image i see coe is flashed ok and connection is dropped after run app. This is normal if your code use power down modes as STOP or STANDBY, here too NRST line is required.
2022-10-14 04:43 AM
Hi @USolar,
I advise you to refer to this FAQ: How to solve debugger connection issues.
Try "Connect under reset" mode.
Maybe that issue is linked to the ST-Link firmware version.
So, try to upgrade the ST-Link firmware version, then disconnect and connect your board.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-10-14 05:59 AM
KDJEM.1 (ST Employee), thank you for reply.
I passed through offered above FAQ Section in the beginning of my issue.
I can connect only when Reset button on board (MCU's NRST pin to GND) is pressed.
After such connection It is able to make Mass Chip erase as well.
But, during flashing, the flash proceess has interrupted and connection to the MCU was lost.
Iwan
2022-10-14 06:12 AM
Send your PCB design or picture. Problem can be in power supply too. Try to measure noise in power suply lines by osciloscope.
2022-10-14 07:39 AM
Seems your code use pins for SWD interface. No problem, but for reprogram this situatio code, STLink need control NRST pn with wire 4. Normal SWD need GND DATA and CLOCK only.
Dongle from china dont have connected NRST need customize ...
2022-10-15 04:00 AM
Below is the Schematic of the Power module for my PCB.
Also, I measured the Power lines with an Oscilloscope, which showed 3.14VDC.
The board has a supply from the dongle during flashing.
2022-10-15 04:03 AM
MM..1 (Community Member) thank you for your reply.
I don't use the pins for SWD Interface.
Below, is the MCU Pinout view for the Test flashing.
2022-10-15 09:06 AM
Ok then from your first image i see coe is flashed ok and connection is dropped after run app. This is normal if your code use power down modes as STOP or STANDBY, here too NRST line is required.
2022-10-19 06:35 AM
I found the issue's reason.
As I said, this is my first Custom board.
I did a mistake in the design of the PCB, didn't connect the BOOOT0 pin to the GND via a 10k resistor.
So, I solder a 10k resistor to the BOOT0 pin and gnd and the problem disappeared.
Now, I can flash, and read the MCU without the Reset button pressing.
Thanks to everyone for your help.