2020-05-13 01:00 AM
I'm trying to get a nucleo-H7A4 getting to run my code.
Only I got this message now:
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-LINK SN : 003A001A3038510234333935
ST-LINK FW : V3J6M2
Voltage : 3.31V
Error: No STM32 target found!
2nd connect tentative with a lower frequency (8MHz)
ST-LINK SN : 003A001A3038510234333935
ST-LINK FW : V3J6M2
Voltage : 3.30V
Error: No STM32 target found!
Encountered Error when opening C:\ST\STM32CubeIDE_1.0.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.3.0.202002181050\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
Is the device now bricked? Any how is this possible with only programming flash?
Solved! Go to Solution.
2020-05-13 07:01 AM
I've had precisely this problem.
Solution is to connect BOOT0 high. Then power on. Connect a second USB cable to CN13. Run STM32CubeProgrammer and connect over USB - not ST-LINK. You should get a connection. Then erase all memory on the H7A3. Power off. Remove BOOT0 connection. Power-on and you should find ST-LINK works again.
Why? - Who knows - a bug in ST-LINK V3?
2020-05-13 03:59 AM
Try connect under reset.
2020-05-13 04:34 AM
I did, the device doesn't start programming when the reset button is pressed.
When I release the reset button I got the same error message.
2020-05-13 07:01 AM
I've had precisely this problem.
Solution is to connect BOOT0 high. Then power on. Connect a second USB cable to CN13. Run STM32CubeProgrammer and connect over USB - not ST-LINK. You should get a connection. Then erase all memory on the H7A3. Power off. Remove BOOT0 connection. Power-on and you should find ST-LINK works again.
Why? - Who knows - a bug in ST-LINK V3?
2020-05-13 07:31 AM
Thanks!. That solved it.
2025-02-13 02:05 AM
A possible explanation (and slightly simpler remedy) for this is mentioned in the manual, section 7.4.8:
The remedy on page 26 can be interpreted as just:
- Connect CN11 pins 5 (BOOT0) and 7 (VDD).
- Start Cube Programmer with USB cable attached to CN1 as you would normally.
- Full Chip Erase
- Power down.
- Disconnect CN11 pins 5 and 7.
2025-02-13 02:20 AM - edited 2025-02-13 02:21 AM