2024-05-02 03:57 AM
Hello,
I'd kindly ask for some help on determining exactly which MCU pin is connected to STMod+ extension board.
Which pins exactly are connected to STMod+ pins 2 and 3 ?
It seems like two choices for both pins, but I'm not sure how to check/modify which comes to STMod+ connector?
I guess from schematic that PI2 amd PB15 are connected to pins 2 NS 3, but that would mean that I don't have
USART device on STMod+ connector ?
Thanks in advance,
regards.
Solved! Go to Solution.
2024-05-03 02:41 AM
Agree, not usable for Clickboards, but usable for breadboard connections and prototyping.
Regards.