cancel
Showing results for 
Search instead for 
Did you mean: 

Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discover

younginpark
Associate II

I am using the STM32F407IGT6 chip. However, when I connected JTAG, the symptoms shown in the picture appear. So I have completed the VDD or continuity test. Can you tell me the circuit diagram and the reason?

STM32Programmer.PNG

schematic.png

  

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome @younginpark, to the community!

the pull resistor at BOOT0 have to be connected to GND instead of VDD.

BTW: the pull-up at NRST is not necessary, see the description of NRST in the respective reference manual.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I tried connecting BOOT0 to nothing or connecting it to GND.
NRST(R8) is not connected to anything other than a pull-up resistor.

Boot1 is currently in a null state with nothing connected.

I tried connecting BOOT0 to nothing or connecting it to GND.
NRST(R8) is not connected to anything other than a pull-up resistor.
Still not working. Do you know why?
Boot1 is currently in a null state with nothing connected.