cancel
Showing results for 
Search instead for 
Did you mean: 

Can't find STM32-F411E Discovery Board VCP

gammmmmm
Associate

Moved from: https://community.st.com/t5/mems-sensors/gyroscope-l3gd20-on-stm32-f411e-discovery-board/m-p/742133#M24523 as this starts a new question:

 

Thanks for replying! @waclawek.jan @Andrew Neil 
I have found the necessary libraries in the cubeF4 packages, But i'm facing another problem.
I can't find the com port of the device on the device manager, I installed the stlink driver and It still doesnt appear.
I also tried to configure the usb peipheral as virtual COM but it still doesnt work.

11 REPLIES 11

Don't forget to mark the solution in your other thread.

 


@gammmmmm wrote:

I can't find the com port of the device on the device manager


Which "device" are you referring to?

There are two on this board:

  1. The ST-Link;
  2. The STM32-F411E target.

AndrewNeil_0-1731445021044.png

 

Pavel A.
Evangelist III

Older ST-LINKs do not have VCP. You cannot find the VCP in device manager probably because there isn't any.

 

Indeed the User Manual makes no reference to a VCP

https://www.st.com/en/evaluation-tools/32f411ediscovery.html#documentation

Although the schematic does show UART connections to the ST-Link:

AndrewNeil_0-1731445687171.png

AndrewNeil_1-1731445768273.png

https://www.st.com/en/evaluation-tools/32f411ediscovery.html#cad-resources 

 

@gammmmmm does the ST-Link show as a debugger in your Device Manager?

AndrewNeil_2-1731445932236.png

See: https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105/highlight/true#M956 for troubleshooting tips

 

 

SofLit
ST Employee

Hello,

Are you sure you are using a data cable and not a charging cable?

If you try to connect with STM32CubeProgrammer, are you able to connect to the MCU?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

@Andrew Neil wrote:

Indeed the User Manual makes no reference to a VCP


The Product Page overview also says nothing about VCP:

https://www.st.com/en/evaluation-tools/32f411ediscovery.html#overview

 

Perhaps @SofLit can confirm whether or not there is one?

Karl Yamashita
Principal

That STM32F411 board looks to be similar to the STM32F4DISCOVERY. 

The STM32F4DISCOVERY's on board ST-Link doesn't incorporate a VCP. I would take a guess to say the STM32F411 doesn't either.

I used a Mikroe board which added a UART port, CAN and Mikro Bus. https://www.mikroe.com/stm32f4-discovery-click-shield

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

The Original STM32F4-DISCO lacked mbed and the VCP/MSC, smaller STM32F103

Later mbed was adopted, and a newer/larger STM32F103 was employed

The STM32F4-DISC1 iteration escaped the ST-LINK/V2-1 VCP to pins, but did not change the circuit to get them to the STM32F407

The NUCLEO-F4 boards DON'T have this issue because they came out to support mbed.

But the NUCLEO-64 boards typically shared the VCP UART and ARDUINO D0/D1 pins

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Andrew Neil wrote:


The Product Page overview also says nothing about VCP:

https://www.st.com/en/evaluation-tools/32f411ediscovery.html#overview

 

Perhaps @SofLit can confirm whether or not there is one?


Yes I think VCP is not supported in that board as it was not stated in the user manual UM1842.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Hey, it appears as STM32 STlink

gammmmmm_0-1731580576676.png