cancel
Showing results for 
Search instead for 
Did you mean: 

Can't find STM32-F411E Discovery Board VCP

gammmmmm
Associate

Moved from: https://community.st.com/t5/mems-sensors/gyroscope-l3gd20-on-stm32-f411e-discovery-board/m-p/742133#M24523 as this starts a new question:

 

Thanks for replying! @waclawek.jan @Andrew Neil 
I have found the necessary libraries in the cubeF4 packages, But i'm facing another problem.
I can't find the com port of the device on the device manager, I installed the stlink driver and It still doesnt appear.
I also tried to configure the usb peipheral as virtual COM but it still doesnt work.

11 REPLIES 11

Yes, St-Link. but without a VCP.

 


@gammmmmm wrote:

Hey, it appears as STM32 STlink

gammmmmm_0-1731580576676.png

 


They are two different things:

STLINK is seen in the list of USB devices, while Virtual comport is listed in Ports (COM & LPT).

This is an example with a NUCLEO board. Each function is listed separately.

SofLit_0-1731581468226.png

So in your case the STLINK in that board doesn't feature VCP (Virtual CompPort). Need to use an external USB/UART like this one: https://2btrading.tn/accueil/1758-carte-convertisseur-cp2102-usb-vers-ttl-serial-uart-pour-arduino.html

Hope it helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.