Availability of evaluation board for Target MCU STM32F765XX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-22 1:23 AM
Please let me know if there is any evaluation board available from ST for target MCU STM32F765XX.
Thanks,
Solved! Go to Solution.
- Labels:
-
ST boards
-
STM32F7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-25 3:01 AM - edited ‎2023-12-25 7:24 AM
Hello @rdevisetti ,
It depends on your needs and what do you plan to evaluate.
- You can consider NUCLEO-F767ZI board for "basic evaluations" it's cheaper than the other boards.
- If you plan to evaluate more advanced features, you can consider STM32F769 Discovery board. For example to use the display / SDcard etc ..
- For more features to access relatively the full MCU features, you can consider STM32F769-EVAL board. For example to use an external NOR FLASH or SRAM via FMC or use CAN etc ..
Refer to the corresponding user manual for each board for more details:
UM1974: STM32 Nucleo-144 boards
UM2033: STM32F769I-DISCO board
UM2035: STM32F769-Eval board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-22 1:33 AM
Well, the STM32F765 is identical to the STM32F767 except for the missing LCD TFT controller, so you can use the NUCLEO-F767ZI as a development platform.
Hope that helps?
Good luck!
/Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-24 8:30 AM
Can I also use STM32F769I-EVAL instead of NUCLEO-F767ZI? Please clarify with details.
Thanks, in advance.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-24 12:39 PM
What aspects are you looking to evaluate? Most of the F7 boards would be reasonable proxies. There are several NUCLEO, DISCO and EVAL series boards depending on the functional coverage and budget.
Also ones out of the Chinese markets that breakout pins and functionality.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-24 11:58 PM
Hello
1. there are no board products in ST web based on STN32F765XX silicon dedicate.
2. there is a NUCLEO product NUCLEO-F767ZI
3. 765 VS 767, from the datasheet, they are with the same core and similar performance.
to sum up, no board product available for STM32F765XX, but you may consider NUCLEO-F767ZI as a candidate if you want to evaluate a solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-25 3:01 AM - edited ‎2023-12-25 7:24 AM
Hello @rdevisetti ,
It depends on your needs and what do you plan to evaluate.
- You can consider NUCLEO-F767ZI board for "basic evaluations" it's cheaper than the other boards.
- If you plan to evaluate more advanced features, you can consider STM32F769 Discovery board. For example to use the display / SDcard etc ..
- For more features to access relatively the full MCU features, you can consider STM32F769-EVAL board. For example to use an external NOR FLASH or SRAM via FMC or use CAN etc ..
Refer to the corresponding user manual for each board for more details:
UM1974: STM32 Nucleo-144 boards
UM2033: STM32F769I-DISCO board
UM2035: STM32F769-Eval board