2020-06-29 10:07 PM
Dear Sir/Madam,
I am going to install STM32CUBEIDE_1.3.0_5720(Windows based) on my system .In the initial phase of installing ,I was asked to choose or select :
SEGER J-Link drivers
ST-LINK drivers
ST-LINK servers
For your further info, it should be mentioned that: I installed before: "STM32 ST-Link Utility" (last version from ST website) on my computer to use ST-Link V2 programmer .
Do I really need to choose and select: SEGER J-Link drivers,ST-LINK drivers,ST-LINK servers
on my system?Were they installed by "STM32 ST-Link Utility previously" on my system or NOT?If I install them,will I face any conflict or problem with my computer?
I really appreciate your attention.
Solved! Go to Solution.
2020-06-30 02:38 AM
Hi,
Which package you choose to install is up to you and which use cases you expect to work when it comes to debug/flash operation inside CubeIDE.
If you expect debug to work, you should however install all of them. OK, you can skip SEGGER if you know that you will not use a SEGGER probe nor the ST-LINK on-board SEGGER firmware. Then this package is ~110MByte. So maybe not an issue to install...
To my knowledge, there has not been any reports of conflicts between the drivers bundled with CubeProg / St-LINK Utility / CubeIDE. So I would simply rely on the CubeIDE bundled stuff which I assume may be of later version.
2020-06-30 02:38 AM
Hi,
Which package you choose to install is up to you and which use cases you expect to work when it comes to debug/flash operation inside CubeIDE.
If you expect debug to work, you should however install all of them. OK, you can skip SEGGER if you know that you will not use a SEGGER probe nor the ST-LINK on-board SEGGER firmware. Then this package is ~110MByte. So maybe not an issue to install...
To my knowledge, there has not been any reports of conflicts between the drivers bundled with CubeProg / St-LINK Utility / CubeIDE. So I would simply rely on the CubeIDE bundled stuff which I assume may be of later version.
2020-07-02 07:44 AM
Thank you matte for your reply .