cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 LPTIM compare mode

catalin78
Associate

Hi, I use STM32CubeMX 6.10.0 and I have a STM32H7 CPU.

The LPTIM is a frequency counter that can give an ISR when the

counter reached a specified value; after reaching this value it starts

again from zero (ARR mode), or it continues towards the max value

on 16 bits and then starts again from zero (CMP mode)

My question is: can I configure from CubeMX this LPTIM in CMP mode?

To me it seems there is no settings for this, whatever I do it's still in ARR mode ..

the solution would be to make manual code changes ?

 

1 ACCEPTED SOLUTION

Accepted Solutions
Saket_Om
ST Employee

Hello @catalin78 

For your application you can just set the mode to "Counts internal clock event".

Saket_Om_0-1738682249588.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

View solution in original post

2 REPLIES 2
Saket_Om
ST Employee

Hello @catalin78 

For your application you can just set the mode to "Counts internal clock event".

Saket_Om_0-1738682249588.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

yes, this is my setting. It didn't generate exactly the code I needed, but I found a solution changing some user code defined sections (cause my problem was that initially i modified generated code)