2021-10-12 12:39 AM
你好,关于STM32G030在PCBA�?��?上的在线烧录,想知�?�是下载什么软件�?�烧录? 用的工具是ST-Link V2�?�以�?�?还有如果芯片程�?加密�?护了�?怎么解�?�?能用ST-Link V2�?�烧录?
或者�?�以推�??�?�外一款USB在线烧录工具能满足�?求, 谢谢。
2021-10-12 1:15 AM
Hello @Ayang.1
Let me first welcome you to the Community :)
I've translated your question using a Google translate tool to increase the chances of getting you a reply from community members, since the majority interact in English. Here is the translation of your post:
"About the online programming problem on the STM32G030 chip board
Hello, regarding the online burning of STM32G030 on the PCBA board, I would like to know what software is to download for burning? Is it possible to use ST-Link V2? And if the chip program is encrypted and protected, how can I unlock it to burn with ST-Link V2?
Or you can recommend another USB online burning tool that can meet the requirements, thank you.
"
To unlock your board via ST-Link Utility, you can download and install STM32 ST-LINK utility (but it's replaced by STM32CubeProgrammer), then open the app, connect the board and reset the Option Bytes.
Although It's recommended to use STM32CubeProgrammer (STM32CubeProg), a programming tool available in graphical and command-line versions for programming STM32 products. You can "connect under reset" and erase the flash.
If your question is answered, please select the answer as “Best�? as this will help other users to find answers faster.
If you still have issues, don't hesitate to come back to the Community.
Imen
2021-10-12 1:47 AM
I try to connect PCBA board with programer tool STlink-V2, but show can't connect target STM32G030XXX from STM32CubeProgrammer software interface. see below image.But I try STM32F030XXX can connect the target, please let me know what is the problem for STM32G030XXX?
Check if STlink-V3 can meet this requirement?
2021-10-12 3:07 AM
Have you upgraded the ST-link firmware? go to ST-LINK > firmware update or through this Link STSW-LINK009.
Maybe you should check if the MCU is correctly powered and connected in the right pins !
Imen
2021-10-12 6:24 PM
Yes, I already upgraded the latest FW successfully, see below image.
I can make sure the pin contact is very good and powerd on by 3.3V from STlink-V2 tool. Since this tool has been using STM32F030XXX progrmaming, only changed to new MCU type STM32G030XXX, other no change. programming point is same as STM32F030XXX.
I checked PCBA TopBand supplier, was told if the STM32G030XXX was encrypted protection after programming by them, STLink-V2 tool can't be used, if no encrypted protection STLink-V2 tool can do programming. But you mentioned even encrypted also can be used for unlock and programming, please help, thank you!
2021-10-12 7:00 PM
I used STLink Utility also happened same error, can't connect the target. I am curious that why STM32F030XXX encrypted protection can connect the target with Stlink-V2 tool, while STM32G3030XXX can't connect the target? What is the difference?
2021-10-12 7:31 PM
G0 is designed for very low pincount packages, compared with F0.
Check boot0, swdio, swdclk and nrst pin configuration and usage in flashed application.
2021-10-12 7:39 PM
Sorry, I selected under reset mode can connect the device but show "data read" failed, see below image. This was casued by third party chip was encrypted protection?
2021-10-12 8:23 PM
But I can't find the unlock item from STMCubeprogrammer menu. Do you know how to unlock encrypted protection STM32G030XXX?
2021-10-14 10:24 AM
Hi @Ayang.1 ,
Is the read protection byte checked? maybe try uncheck it.
Imen