ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem with STEVAL-D25R16B and STSW-ST25R010

I was trying to setup the software (ST25R010) for NFC reader, and not only was I unable to setup the software but I realized the board malfunctioned at some point. The board initially worked fine but now it shows a reversed error message and I cannot...

Etix by Associate II
  • 517 Views
  • 3 replies
  • 1 kudos

Resolved! Questions on Formatting ST25DV Tags for NDEF

For our NFC project, we are developing a mobile application that supports both iOS and Android. We are using React Native along with the react-native-nfc-manager library. Some of the core features include reading and writing raw memory blocks as well...

shahbaz by Associate II
  • 804 Views
  • 1 replies
  • 0 kudos

Resolved! ST25R3911-B: Can't receive large data blocks on FTM (ST25NFC_Embedded_Lib_ST25R3911B_1.8.0)

Hello everyone. I'm currently developing and testing an embedded C software for microcontroller STM32L476 integrated on board ST25R3911B.In order to better understand FTM and its features, I'm trying to use a ST25NFC_Embedded_Lib_ST25R3911B_1.8.0 dem...

pa0grg by Associate III
  • 779 Views
  • 7 replies
  • 0 kudos

Resolved! How to reduce the current of ST25R3920B

Hi all,I now use ST25R3920B as a card reader on the official nucleo nfc08A1 of ST to read cards. However, I found that when the card was detected by 3920B, the current increased to 300mA, but the maximum current borne by PCB was 350mA.Can I reduce th...

Resolved! ST25DV64K read more than 64 blocks at once

I use the Flutter NFC Kit library.I enter the password and then use: Extended Read Multiple Blocks"2033XXXXXXXXXXXXXXX00003F00"Request_flags -> 20Extended Read Multiple Block -> 33UID -> XXXXXXXXXXXXXXXFirst block number -> 0000Number of blocks -> 3F...

Greidimar by Associate III
  • 215 Views
  • 1 replies
  • 0 kudos

Resolved! Looking for a suitable antenna for ST25R100-CMET

Updated the title to be inline with ST community rules. Hi all! So I am looking for a standard antenna which would be suitable for ST25R100-CMET (IC Reader 13.56MHZ 24 UFQFN). This will be used in an alarm module with a lock, so please suggest! Thank...

vibrao by Associate
  • 1562 Views
  • 2 replies
  • 1 kudos

Resolved! Ambiguous ST25DV-I2C StMicro literature.

The last few lines of  StMicro’s ST25DV-I2C  low power application note (high lighted) are ambiguous. Does “ST25DV-I2C” have the ability to read/write EEPROM without power applied between pins VDCG and GND? (YES/NO)  Our desired application needs to ...