ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Example of using the new iOS 13 CoreNFC

does ST have examples of using the new NFCTagReaderSession which works with M24LR16E and up. examples of using NFCISO15693Tag protocol methods: readSingleBlock, writeSingleBlock, lockBlock, readMultipleBlocks, writeMultipleBlocks, getMultipleBlocksSe...

dmurphy by Associate II
  • 3253 Views
  • 8 replies
  • 1 kudos

Resolved! ST25R3916B self-tests fail

HiI'm trying to communicate from a STM32WB5MMG via a ST25R3916B to a ISO14443-A tag.I use the X-CUBE-NFC6 RFAL library with ST25R3916B, RFAL_FEATURE_NFCA and RFAL_FEATURE_T2T set.Both ST25R self-tests fail:ST25R_SELFTEST returns RFAL_ERR_TIMEOUTST25R...

DaDu by Associate II
  • 1107 Views
  • 8 replies
  • 0 kudos

Resolved! ST25dv16k enable the energy harvesting

I am new to NFC. Currently, I have an ST25dv16k NFC. I wrote the EEPROM using the example Arduino code provided in GitHub. I am trying to enable the energy harvesting feature. How will I assign EN_MODE register to 0. Please help.

HM J.1 by Associate
  • 954 Views
  • 2 replies
  • 0 kudos

Resolved! ST25R3911DiscoComm.dll 64-bit

Dear ST Community,I have just downloaded the software https://www.st.com/en/embedded-software/stsw-st25sdk001.html and I am trying to run the python demo DLL_Demo.py. When I attempt to load the DLL there is an exception: ST25R3911_Dll = windll.LoadLi...

benjacam by Associate
  • 355 Views
  • 1 replies
  • 0 kudos

Resolved! Writing to and reading from ST25DV04KC through i2c.

Hello ALL.I am reading this from the ST25DV04KC datasheet:"During the internal write cycle, the device disconnects itself from the bus, and writes a copy of the data from itsinternal latches to the memory cells. The maximum I²C write time (tw) is sho...

baranovus by Associate III
  • 449 Views
  • 2 replies
  • 1 kudos