Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L052R8 Watchdog Timer Issue

I have configured the watchdog for the maximum duration possible, i.e, 1.7 sec. void watchdog_init(void){CLK_ICKCR |= CLK_ICKR_LSION;IWDG_KR = 0x55; IWDG_PR = 6; IWDG_RLR = 0xFF;IWDG_KR = 0xCC; }But it seems to be resetting in around 26 - 28 ms. I ha...

Resolved! Use of EV-L99LDLH32GEN development board

1. Regarding the development board: Does EV-L99LDLH32GEN require an external driver to work? Or does the development board come with its own driver chip? 2. In addition to driving LEDs, can it also drive other loads?   This post has been translated f...

Jing_H by Associate
  • 1155 Views
  • 1 replies
  • 0 kudos

Resolved! SGS digital sound generator M114B1 chip

Is there anybody who have a copy of that old ('80) sound generator, marked by SGS, used in some old italian keyboards like the GEM ones? I have references only for the M114A, but that is bigger (48 pin against 40 pins) and seems to be a bigger versio...

ACont.1 by Associate II
  • 2780 Views
  • 5 replies
  • 1 kudos