Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S001J3 setup for AIN2

This is driving me crazy. First time with this processor. I have AFR2 and NAFR2 set properly for AIN2 operation. I can verify that in the watch window and the disassembly window looks like it is working as expected. If I change the channel to AIN7 I ...

STVD weird behavior and debug context crash

After many years without problems, now my STVD is acting weird.It shows different behaviors running as user and adminAs user:The Open Workspace file selector pup-up file type is set to show only .exe files (it should be .stw files)When I start debugg...

gabs by Associate II
  • 1676 Views
  • 0 replies
  • 0 kudos

Resolved! I2C PROBLEMS

Hi there!First, I need to declare my frustration with CUBE IDE complexity. My code is not for blinking a LED or test one button, but a complex code that involves an 7 inch LCD, EEPROM, TEA6686 PLL, DS3231 RTC, DS18B20 temperature sensor and so on, It...

m-a-c-f by Associate III
  • 2159 Views
  • 3 replies
  • 0 kudos