Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm8s flash entire new program - how?

Let's assume I have a program that exposes a serial interface for commands and one such command is "load new program".  I upload the new program as hex strings and the old program writes this to flash and the resets.  Hopefully at this point the new ...

Resolved! Does ST-Link/V2 support STM8S103F3 ?

Dear All,I started working on the STM8S Mcu's recently. Here I have some basic queries.1)By using this ST-Link V2 in circuit debugger and programmer. (ST-LINK/V2 - ST-LINK/V2 in-circuit debugger/programmer for STM8 and STM32 - STMicroelectronics) Can...

Halt mode and Current consumption

Hi, I have a STM8S001J3. I want to put my uC in halt mode because I'm on battery. The problem is that halt mode consume around 1mA when the interrupts are enabled. I need interrupts to wake up from halt mode with my GPIO pin so I can't disable it.I t...

MSL

Hello , Is it possible that I have MSL 1 on a label even though everywhere else says that this Part is MSL 3?

Diwo72 by Associate
  • 1323 Views
  • 1 replies
  • 0 kudos

USB Power Delivery using STUSB1602 library

Hi there,We are using the STUSB1602 for charging 10W devicesI'm looking to download the STSW-STUSB010 library, It seams that the STSW-STUSB010 library is not available, also from web search, there is version 015  some sites claim that the library is ...

GalBTM by Associate II
  • 2199 Views
  • 3 replies
  • 0 kudos

LittleFS with M95256-DRMN3TP EEPROM Device

Hello, I am using M95256-A125 EEPROM device as NV data storage in our application. SPI communication is used to communicate from host to EEPOM device. EEPROM  Device has page size 64bytes but little-fs expects minimum page size as 104 bytes.  My ques...

Dev001 by Associate
  • 831 Views
  • 0 replies
  • 0 kudos

Resolved! diode reference BUZ GP642 or BUZ Z338

 Bonjour à tous, quelqu'un pourrait m'aider à trouver la référence de cette diode ou un équivalent, car je ne trouve pas la fiche technique sur internet, je vous remercie d'avance pour vos réponses 

IMG_20241125_150332.jpg
MAOU by Associate
  • 2220 Views
  • 3 replies
  • 4 kudos