Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TDA7566

We are working on one of our project which previously using TDA7566 IC. Can anyone suggest any pin-to-pin compatible IC for TDA7566? Are the following IC's are compatible - TDA7580, TDA7388, TDA7850? I would like to know more about the 3 pins (pin nu...

Raj23 by Associate
  • 942 Views
  • 1 replies
  • 1 kudos

Resolved! STM8 vs Cortex-M0/0+ in a new project

 I am studying a project that requires a very small microcontroller. It will only drive analog and digital ports, but we need the I2C protocol and maybe even CAN. I was advised to use the STM8, but I am not comfortable with this choice. And I wanted ...

L9369 reference design

L9369 Control Signals for Redundant Safety Switch-off Path From μC—Are these 4 signals be connected together?or connect ACT_OFF_LS1_A and  ACT_OFF_LS2_A  together ?    connect ACT_OFF_LS1_B and ACT_OFF_LS2_B together ?Is there reference design for Au...

haihun by Associate II
  • 834 Views
  • 1 replies
  • 0 kudos

Resolved! Default I2C address of ST33KTPM2X

Hi, In the ST33KTPM2X datasheet is mentioned that the I2C device address is configurable in the range of 0x08 to 0x77, but what is its default after power-up ... it is not mentioned in the datasheet. A STSafe application note suggests 0x2E, is that c...

LMaarsen by Associate
  • 1546 Views
  • 2 replies
  • 0 kudos