Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN Bus

Posted on April 10, 2012 at 15:31I try to use an exemple by KEIL, but when i try to debug it doesn't work, my main is : ''/******************** (C) COPYRIGHT 2007 STMicroelectronics ******************** * File Name          : main.c * Author       ...

stm8 uart1

Posted on October 29, 2012 at 07:25hello, please can someone one help me with a uart problem on the stm8s i use a crystal of 14.7456 Mhz , also i do the change of the clock system, see the atached program. the uart1 is initialised as, pa4 and pa5, ...

stm8s20x series MODBUS RTU and ASCII

Posted on October 20, 2012 at 04:10HiI looked at google  MODBUS RTU and ASCII for some source code for stm8 but i could not find any source code for stm8 series... 1. Is there any source codes for stm8 series?2. When a device is connected to stm8 ua...

irmakci by Associate II
  • 2079 Views
  • 2 replies
  • 0 kudos

help with st10 flasherV24b,can not reload monitor

Posted on March 02, 2012 at 02:02Hi, I try to use st10flasher tool(Flasher_V24b). In windows xp works but when I try to read the mcu (st10f269) with dump I can save the dump only in text format. If I try to save in hex, the program report target not...

leven333 by Associate
  • 1023 Views
  • 1 replies
  • 0 kudos

STM8S

Posted on October 22, 2012 at 12:14hello, please is there a sort of stm8s assembly language available who convert a 16 bit binary  to 5 bcd  code many thanks marc debruyne

Interrupt and PEC handling

Posted on October 22, 2012 at 17:16I've read the manual like a billion times, and still can't find a very conclusive answer.  If the CPU instruction pointer is is an interrupt service routine, and a PEC transfer is requested.  What happens?  Does i...

drobison by Associate II
  • 890 Views
  • 0 replies
  • 0 kudos

RAM memory issue on STM8L151G6

Posted on September 28, 2012 at 17:41RAM memory issue on STM8L151G6When using the RAM there are five addresses that I cannot change by software: 0x102, 0x12F, 0x237, 0x24D and 0x2A9. I am using the following test code; for (i=(unsigned char *)0x000;...