Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VNH3SP30-E

Posted on October 11, 2012 at 15:00I would like to use a VNH3SP30-E to control the rotation of a dc motor. No PWM. My question is about the inputs, INA, INB, ENA and ENB. Do I need pullup and/or series resistors for these inputs? Can I just tie the ...

rcolman by Associate
  • 1374 Views
  • 1 replies
  • 0 kudos

Flash Dump

Posted on October 09, 2012 at 10:59I have this problem with a ST10F269 mounted on an automotive ECU: the flash dump and programming go straightforward, even the programming with different software releases is OK.What I can't do is editing the data e...

STM8L Sleep Speed

Posted on October 08, 2012 at 08:40 OK, title sounds really weird, but I'm really curious about the low pawer state switch speed of the STM8L micro. I'm doing some tests about switching to LSE and back to HSI, waiting for stablization etc. I...

Debugger Stopwatch

Posted on September 28, 2012 at 09:52Hi Guys,Do we have a stopwatch feature within STVD? I'd like to measure passed time between two breakpoints as time (us, ms) and cycles.I know there are simulators with MPLAB and IAR IDE with this function but co...

chibiOS and IAR

Posted on September 25, 2012 at 05:48Hi all,Does everybody have examples chibios base on IAR of stm8? Now cosmic limited 8k, so I want to change to IAR Thanks and best regards Thinh

np1 by Associate II
  • 824 Views
  • 0 replies
  • 0 kudos

EWSTM8 of IAR - problems with debugging

Posted on September 21, 2012 at 10:33Dear,In the past I published here in the forum a question about EWSTM8 problems.I have been in touch with IAR on that and now I have their Beta version. This beta version has solved a problem with crashes as resu...

elil by Associate III
  • 3638 Views
  • 0 replies
  • 0 kudos

Software Update on STM8

Posted on September 12, 2012 at 12:40I am working on a low density STM8S with 8Kbyte flash memory. I need to accomodate a main software and a recovery software. I do not need any special bootloader as I am planning to make the software update as pa...

spveer by Associate II
  • 1934 Views
  • 3 replies
  • 0 kudos

ICP and IAP: Linker

Posted on September 18, 2012 at 17:21 Hi, Is it possible to program only part of the flash memory using ICP? I have STM8 programmed with bootloader using ICP where UBC is protected from 0x8000 to 0x8fff. Now when I try to...

spveer by Associate II
  • 768 Views
  • 0 replies
  • 0 kudos

TIM3 wrong counting?

Posted on September 04, 2012 at 17:14I need to generate a 20 ms interrupt into my firmware. HSE is 16 Mhz with STM8S208. I put this initialization code into my firmware to accomplish that through the use of TIM3: #define PRESC TIM3_PRESCALER_32     ...