Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8

Posted on December 19, 2012 at 16:45Respected All:           I new for STM8s003k3 and i compile the peripheral coding like GPIO,USART ..But i did not not got Hex file.And i use the STVD compiler.Can any one tell me how create a hex file.i Read the P...

STM8L DAC+DMA+TIM4

Posted on October 23, 2012 at 13:02hello, i'm trying to play raw pcm (22050 Hz, 8 bit unsigned, mono) from sd card to DAC through DMA, with ring buffer. everything works perfectly when i'm using TIM2 as interrupt source (at 22050 Hz) and DAC's softw...

new in this MCU

Posted on July 07, 2012 at 14:41hello, i have done other MCUs like 8051, PIC, AVR. now i want to use this MCU.  i want to start with STM8Sxxxx series..please suggest me how to start.thanks in advance.

How to correctly configure UART pins in asembler

Posted on December 17, 2012 at 22:07I'm willing to init UART in asm and not sure is it required to configure specific IO port pin as  output pin with Px_DDR and only then then I can use UART_TX  or the pin configures in output type automatically wh...

OPTOCOUPLER CTR:1

Posted on December 10, 2012 at 12:49I used the eDesignSuite for my first time. The design was a flyback converter and the feedback to the controller is solved using an optocoupler but with no reference. It's only specified an OPTO with CTR:1. Can an...

rciurans by Associate
  • 1610 Views
  • 1 replies
  • 0 kudos

STM8 CAN, CAN bootloader

Posted on November 29, 2012 at 14:24Hello! Now I'm in search of design of my project and I really going to use STM8s208 MCS's. Im'm new to STM8 at all.I need a wired controller network, with about of 20 devices. Every device should be able at any ti...

urvindt by Associate
  • 900 Views
  • 0 replies
  • 0 kudos