Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

COSMIC IdeaSTM8 32K Dev Tool

Posted on August 24, 2013 at 22:40Hello, I recently downloaded the IdeaSTM8-32k dev tool from COMSIC and have trouble saving newly entered C files.I can successfully compile and link the example code provided by COMSIC. When I attempt to include an ...

mark by Associate
  • 674 Views
  • 0 replies
  • 0 kudos

Moveable Code Feature : Change rom location

Posted on August 23, 2013 at 02:54Hi sir,        we have a project. This issue is that one project include application code and bootloader code.We already study the COSMIC datasheet about the Moveable Code feature. But we can’t find that how to chan...

robinsen by Associate
  • 566 Views
  • 0 replies
  • 0 kudos

STM8L SWIM pin set up?

Posted on August 20, 2013 at 13:43How should PA0 be set up for the SWIM interface? Input? Output? Shake it all aboutput?Pretty fundamental Q I'd have thought, but I can't find any info'.plenty of fatuous 'Overviews' about SWIM but little useful info...

CAN Rx interrupt sometimes misses one

Posted on May 02, 2013 at 15:12I am using a STM8S208CB in an embedded device on a CAN network. I have initialized the CAN to use an external 8MHz crystal, 250k baud, and enabled the FIFO message pending interrupt. I have my interrupt function proces...

ST10R167 JTAG

Posted on August 14, 2013 at 18:51I can't find any info about enabling JTAG interface on st10R167, if someone could please tell me anything about it, or point me where to find literature about it, i'll really appreciate it :) #st10-jtag

ST7FLITE29 Write Protect

Posted on July 30, 2013 at 12:08Hi I have a new build PCB with a ST7Flite29 fitted, I cant program the device, I have had to run an external clock signal to Clk In (PB4), the programmer is now reporting ''Write Protected'', how do I get this back, t...

Minimum Interrupt Pulse Width?

Posted on August 12, 2013 at 07:22I am looking at using a STM8S003K3 microcontroller.When a port pin input is configured as an edge triggered interrupt what is the minimum pulse width?  Is this a true edge trigger or is it sampled?I am trying to sav...

STM8 USING STVD & COSMIC COMPILER #error clnk Debug...

Posted on August 10, 2013 at 01:41Can anyone help me with the problem below dotted line?  It seems like I need to set up memory spaces for the Micro Controller.  Is that ? the problem.  If so how do I fix? Thanks! GDN -------------------------------...

greg by Associate II
  • 877 Views
  • 0 replies
  • 0 kudos