Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Spice model for power factor controller L6563s

Posted on December 19, 2014 at 16:57Dear friends,  I am in need of Pspice model for power factor controller L6563.please post ur suggestion for getting the same or is any other way to simulate the power factor correction? #spice-model #l6563h #l6...

rachid2 by Associate
  • 1104 Views
  • 0 replies
  • 0 kudos

IAP bootloader source code for STM8S

Posted on December 18, 2014 at 11:03I�m going through this application note on the ST website: http://www.st.com/web/en/catalog/tools/PF258002The application note states that it comes with source code for an example of an IAP bootloader implementati...

my STVD cant show RAM use

Posted on December 12, 2014 at 04:29HI everyone, i am new to STVD and stm8, cosmic C i follow the thread of this https://my.st.com/public/STe2ecommunities/mcu/Lists/stm81/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/stm81/Output%20Size%2...

FLast.11 by Associate III
  • 1159 Views
  • 2 replies
  • 0 kudos

Need help developing a low level driver for SWIM

Posted on July 17, 2014 at 18:25Dear STM08 Technical supportI am a consultant developing a flash programmer tool for the STM8 that runs on the Teradyne Test Station platform. The end users of this tool will be two high volume users of STM08 devices....

infoinfo9 by Associate II
  • 4911 Views
  • 10 replies
  • 0 kudos

Program four STM8 in parallel.

Posted on December 09, 2013 at 19:15Hi,This is my first post so hi everyone. I would like to program the four STM8 in parallel.I would like to use for this ''STVP_CmdLine.exe'' and ST-Link's V2.  I know that the programmers have different numbers VI...

s_michas by Associate
  • 1048 Views
  • 1 replies
  • 0 kudos

STM8 Programmer tool

Posted on May 17, 2013 at 06:53Hi All, am developing one programmer tool as like ST visual tool , for flashing s19 file.but i dont have API for that . but in website mentioned use PtkApi.cpp but this cant able to download , if any one have idea abou...

rajeeva by Associate
  • 938 Views
  • 1 replies
  • 0 kudos

Urgent: STM8S003F3 reset pin gets damaged

Posted on December 05, 2014 at 14:58I am using STM8S003F3 & attached is circuit. I have connected some switches in pull-up configuration as shown. After some correct operations, I have seen that some of boards stopped working. It was problem 1 as ...

STM8L Interrupt

Posted on October 29, 2014 at 17:07Hello, I'm using the STM8L151 using IAR workbench without ST Firmware Library and I'm trying to use an SPI Interrupt. Unfortunatey it doesn't work. SPI is already running, the receiving flag is set, but i don't get...

ST7540 Eval Board SPI ( urg )!!!!!

Posted on May 22, 2013 at 11:22Hi , I'm using ST7540 Eval Board and i want to send to my Micrcontroller via SPI , 24 bits all at once. The spi i use is 8 bit. Here is an excerpt of my code : volatile uint8_t i=3;     while(i>0){         i--;        ...

elazhar by Associate II
  • 1250 Views
  • 1 replies
  • 0 kudos

STM8 Evaluation- Independent watchdog

Posted on December 01, 2014 at 08:15Hello,  According to reference manual IWDG will not be stopped even after entering HALT mode. Is there a possibility to STOP or PAUSE IWDG for STM8A ? According to STM8AL we can halt IWDG, but STM8AL is not suitab...

kawasthi by Associate
  • 839 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.