Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

eDesign Suite Issue

Posted on December 19, 2016 at 19:22Hi,I am trying to get details for my power supply.My specs are :- Dual OutputOutput 1 :- mailto:17V@1AOutput 2 :- mailto:3.3V@1AConstant VoltageIsolated SupplyFor above specs, I tried to use eDesign Suite, but it...

anuj by Associate II
  • 1089 Views
  • 1 replies
  • 0 kudos

Application note x eDesign (Viper 26LD)

Posted on September 14, 2016 at 11:29I have used eDesign for a buck converter design approach (see attachment). However, I noticed that the suggested components value are not the same as the ones on http://www.st.com/content/ccc/resource/technical/d...

vitor1 by Associate II
  • 3609 Views
  • 7 replies
  • 0 kudos

Timer issue

Posted on December 16, 2016 at 07:11In a timer code, I am facing number of 'missing prototype' errors in the included tim1.c file. Each of the error marks the line starting from 'assert param' ..... in tim1.c file. Do I have to change anything in co...

SPV1040 eDesignSuite doesn't work

Posted on December 06, 2016 at 10:33Dear ST support, I need to simulate circuit for SPV1040. I'm trying to use your eDesignSuite, but it doesn't work (Msg: eDesignSuite requires the latest version of Adobe Flash Player. Click here to verify your cur...

Kaza K by Associate II
  • 1793 Views
  • 3 replies
  • 0 kudos

Resolved! STM timer query

Posted on December 06, 2016 at 13:59We are working on a project based on timer in which we keep facing an error : symbol _TIM1_SetCounter not defined. We have included the header files as well. Thanks in advance.