Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupt not working

Posted on December 21, 2016 at 13:02I am trying to run a code in which timer causes an interrupt and everytime interrupt is generated, a variable h is incremented, but it remains zero in quickwatch window. My code is written below in stvd and cosmic...

Cannot communicate with the tool

Posted on March 21, 2016 at 10:40Hello! I compile sourse code stvp (http://www.st.com/web/en/catalog/tools/PF257522) in visual studio 2015. The program displays an error in console: >>> Programming PROGRAM MEMORY (API) ERROR : Cannot communicate wit...

Why not STM8 wish list?

Posted on January 05, 2017 at 11:54Today I've received email from ST with link to this https://community.st.com/s/feed/0D50X00009bLPmvSAG . So, why there no stm8 wish list? ST has forgot their low child, no any improvements anymore?Anyway, this is m...

Operating Temp. Range

Posted on December 22, 2016 at 09:59(1) Part no. :  STTH108  (2) Part no.: STTH803D (3) Part no.: STTH102 (4) Part no.:  STTH112A (5) Part no.: 1.5KE300A This five part operating temp are not given in datasheet, i need to require operating Temperatu...

Hypoterminal is dead

Posted on September 16, 2010 at 23:33It's not even as if Hyperterminal is a standard part of Windows any more:http://windows.microsoft.com/en-US/windows-vista/What-happened-to-HyperTerminal

EMI fitlter design CC driver

Posted on December 09, 2016 at 16:14Hi,I am designing CC driver using HVLED001A using eDesign tool. Now to complete the design i need to design EMI section which i am not able to do. Please provide some reference guide or something for help me in de...

switching ADC with multi channel

Posted on December 21, 2016 at 11:03Dear allI am using ADC in stm8s105c6. I use ADC1 for two channel for example AIN9 and AIN8.the problem is that when I switch the ADC1 from channel 9 to 8 the output result of the are being swapped.the input signal...