Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN bootloader problem

Posted on March 06, 2017 at 23:07Hello! I can't initialize internal CAN bootloader on stm8AF52A8 with HSE 24 MHz, it is silent.I tested all: �bootloader enable� option byte is set.CAN is OK, i tested it in my program.HSE is OK.Soft on PC is OK, I t...

Turns Ratio Notation 'm'

Posted on March 07, 2017 at 15:21HI:I'm using the eDesignSuite to design an AC/DC transformer that has a secondary at 135 vdc, 40 Iavg.  The listed turns ratio is 550.26m .... why the 'm' ?Here are the transformer details:Transformer Specifications:...

STM8L LCD Register

Posted on October 26, 2016 at 11:18Hi, I'm using the STM8L052R8 for temperature measurement, so using an ADC channel, and then displaying the temperature on the LCD.It would be really handy to be able to clear the LCD Ram memory instead of writing t...

STM8S003F3P6 bandgap reference

Posted on January 19, 2017 at 10:22Hi,Was looking at a recent version of a datasheet for STM8S003F3P6, and there seems to be no comments relating to a bandgap on AIN7.There was mention of it on previous datasheets (I have one from 2014).Is the bandg...

Confused about the transformer Design

Posted on February 25, 2017 at 23:11I am using ST's eDesign Suite for designing power supply. (AC-DC Converter)I contacted the transformer design firm to get my transformer designed. I gave them all the information regarding the number of turns and ...

anuj by Associate II
  • 2235 Views
  • 1 replies
  • 0 kudos