Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L051F3P6 bootloader USART pins

Posted on October 20, 2017 at 09:25Hello! What USART pins of STM8L051F3P6 are dedicated for bootloader, PC5-PC6 or PA2-PA3? Can't find any info about that.The same question about stm8l151c6.Thanks!#bootloader #usart-pins #stm8l051f3

EvgenS Po by Associate II
  • 1420 Views
  • 1 replies
  • 0 kudos

STHV800 rx amplitude problem

Posted on November 06, 2017 at 13:47Hello CommunnityI use the eval board STEVAL-IME013V1Input frequency 40kHzTransmission of a sin 40kHz signal from XDCR8 to LVOUT8 1:1When the piezoelectric element UTR-1440K is switched on to the XDCR8 connector, t...

[ATT]9960

Posted on October 23, 2017 at 19:44Problems counting pulses between 5hz-100hz on STM8s003f3p hikindly help my design.     i am using stm8s003f3p micro-controller. timer 1 input capture unit doesn't work as i intended. i searched web forums and blogs...

Viper06 PSR Wide Input AC to 12 V 0.2A DC

Posted on November 01, 2017 at 09:29How do I change the regulation mode from Secondary to Primary in eDesignSuite?I want to design a low cost 85-265V AC to 12V 0.2A DC isolated flyback converter using the Viper06 with PSR. Tight Voltage Regulation a...

abotha by Associate III
  • 1143 Views
  • 1 replies
  • 0 kudos

Viper 16LD, Non Isolated Buck Regulation issue

Posted on October 26, 2017 at 10:37The output Voltage expected is 6V and output is constant for 110VAC input. But the output is turning ON/OFF for 220V input. Please let me know to resolve this issue. I have followed the ST Design suite for the desi...