Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[ATT]10688

Posted on January 03, 2018 at 23:20stm8s103f2 is not able to program hex my product's board is based on stm8s003f3 mcu(TSSOP 20pin), but there was some problem in providing the chipset,so I bought stm8s103f2 TSSOP20pin instead of buying stm8s003f3.T...

Simon Lee by Associate II
  • 2735 Views
  • 4 replies
  • 0 kudos

STM8 how to change Duty Cycle during running

Posted on January 04, 2018 at 13:40Hello community,i try to programm an code for my experimentation and i have a problem .. my code should change the duty cycle ie. the value of CCR2_V if the value of Convertion_Value_Current exceeds or is below a s...

STM8S001J3 open-drain mode

Posted on December 15, 2017 at 08:22HiI would like to use open-drain mode for PB5 pin of STM8S001J3.GPIO_DeInit(GPIOA);GPIO_Init(GPIOB, GPIO_PIN_5, GPIO_MODE_OUT_OD_LOW_FAST);I do not know why the voltage goes down even if I set it like the code abo...

FORTH for STM8S-Discovery

Posted on July 20, 2010 at 07:08Here is a FORTH interpreter-compiler for Discovery Board.  It is in the form of an assembly file stm8ef.asm.  You can assemble it on STVD and download it to Discovery.  You need a UART connection to Hyperterminal on P...

ting by Associate II
  • 4979 Views
  • 14 replies
  • 0 kudos

is it exist part number stm8s003f2?

Posted on December 27, 2017 at 13:32HelloI bought stm8s003f2 mcu instead of stm8s003f3.The seller told me that it is same as stm8s003f3, after getting it, i tested stm8s003f2 on my custom board by using stlink/v2, but it is not works and there is no...

Simon Lee by Associate II
  • 1403 Views
  • 2 replies
  • 0 kudos

STM8S103 TIM1 Setup External Event Counter

Posted on December 30, 2017 at 02:08Hi,Please, could someone help me to setup TIM1 to count pulses at rising edges? I try this code, but doesn't works.TIM1_DeInit();TIM1_TimeBaseInit(0, TIM1_COUNTERMODE_UP, 581, 0); TIM1_ICInit(TIM1_CHANNEL_1, TIM1_...