Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TL431AID part marking

Hi,Help pls with the "TL431AID"There is "H" symbol on the part (look at the photo pls)What does it mean?There is nothing is the datasheetBest regards and thank UPaolo

0690X000008AYkzQAG.jpg

Resolved! I developed a board with STM8S003F3 (20 pin) controller on it. I'm trying to connect the board via SWIM but i'm not able to. I'm seeking help to connect my own developed board via SWIM using STM8S Development Kit's programmer.

**To confirm connections, I did SWIM on STM8SDiscoveryKit and STM8S103FP6 breakout board & it worked well.My board connections are as follows (STM8S Development Kit's Programmer ---> STM8S003F3): VDD -> pin 9 SWIM -> pin 18 GND -> pin 7 (GND)NRST ->...

NikhilAG by Associate
  • 2294 Views
  • 3 replies
  • 0 kudos

Switch and Power Source Problem_STM8S103F

Hi,I am working on a project, turning on an LED in push-pull mode when a switch in pull-up mode is pressed. The LED only lights up once. I am using IAR and C.Everything works perfectly fine except that, sometimes when the LED is connected to power wi...

Corvette by Associate
  • 858 Views
  • 1 replies
  • 0 kudos

problem on current consumption

Hello,for a battery application, I have some question1) can I have the output pin in stable condition or halt mode puts the output in floating mode?2) I read the current run mode is: 150uA/Mhz + 215uA. At internal 38kHz clock, the total is 220,7uA, n...

FBatt by Associate
  • 816 Views
  • 1 replies
  • 0 kudos

unable to compile stm8 using cosmic compiler?

I'm using the Cosmic Software 4.4.9.0 in ST Visual Develop 4.3.12  I can't compile it.I try to install again but it showing same error.i tried to set root path correct like this C:\Program Files\COSMIC\FSE_compilers\CXSTM8.Can any one help me to solv...

tvenk by Associate II
  • 832 Views
  • 0 replies
  • 0 kudos