Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Choosing an oscilloscope

Hello,I want to buy an oscilloscope to help me learn embedded programming and how to use it(I need that for work) ;).I'm thinking of buying this one: Hantek DSO5072P Digital Oscilloscope, 70 MHz Bandwidth, 1 GSa/s, 7.0" DisplayPlease tell me what do ...

PPopo by Senior
  • 953 Views
  • 2 replies
  • 0 kudos

Why doesn't the COSMIC compiler start?

I downloaded and installed the COSMIC stm8 free compiler (http://cosmicsoftware.com/download_stm8_free.php). I requested and received a license. I copied the license file to the appropriate folder.However, the compiler does not start. It does not sta...

MPele.2 by Associate II
  • 1395 Views
  • 4 replies
  • 0 kudos

STM8L151 crystal with Cload 20pF

Dear,according to the spec. of STM8L151, Recommended load capacitance C=CL1=CL2= 2*CLOAD of crystal, so, if the Cload is 20pF, we should use 40pF for CL1 and CL2?please help to advise if it's ok and if have any other issues?b/rzhang

vzhan by Associate
  • 593 Views
  • 1 replies
  • 0 kudos

We are using L6370 high side switch. 1) We have a doubt/ question regarding the short circuit operation of the IC. 2) doubt regarding timing mentioned in the short circuit operation section.

1) In datasheet, short circuit operation section Section3.4) it is mentioned that ​when output out high side switches is shorted to ground then high side switch follow a time frame & supervise the output state for Ton periode  which is defined by ext...

KBhav by Associate
  • 1054 Views
  • 1 replies
  • 0 kudos