Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Instruction timing changing with memory location?

Hi. I am writing very time sensitive code on the STM8 mostly using assembly. However, I have noticed that sometimes adding one cycle of delay at one point in the code changing the timing of the whole code. I will explain in more detail to clarify. I ...

Chris K by Associate II
  • 1780 Views
  • 4 replies
  • 0 kudos

TIM1_GetCounter() Results

I have initialized TIM1 timer with:TIM1_DeInit();TIM1_TimeBaseInit(16, TIM1_COUNTERMODE_UP, 1000, 0);TIM1_SetCounter(0);TIM1_ITConfig(TIM1_IT_UPDATE, ENABLE);TIM1_Cmd(ENABLE);But calls to TIM1_GetCounter(); return the value 2. I can see the counter ...

When does 'rollover' occur when reading from M24M02

From the datasheet (DocID18204 Rev 10, pg20)...The output data comes from consecutive addresses, with the internal address counter automatically incremented after each byte output. After the last memory address, the address counter “rolls-over�?, and...

Ebail.5 by Associate
  • 862 Views
  • 1 replies
  • 0 kudos

Feedback on STM8 tools

Hi. This is some open feedback on the use of the STM8 tools for a pending project. We are 35 year old OEM design house and about to deploy the STM8S001J3 onto a consumer space product. The assembled PCBs have arrived and now the code development was ...

Mon2 by Senior III
  • 775 Views
  • 0 replies
  • 0 kudos

unable to compile

when i am trying to compile ST Visual develop 4.3.12 with cosmic compiler 4.4.9.0.i am getting this Connection error (usb://usb) [30100]: can't load library.can anyone please help me to solve this problem.

tvenk by Associate II
  • 666 Views
  • 0 replies
  • 0 kudos

about M24M01

A. M24M01-HR(SO8MN)B. M24M01-DF(SO8MN)  1. Replacement between A and B is available?  2. Comparing with A, B is equivalent or higher grade? 3. "24M01FD" as below photo is product 'B'?4. Production of M24M01-HR(SO8N) is still continue or stop?

0690X000008AwEOQA0.jpg
Hyoon.8 by Associate
  • 1038 Views
  • 1 replies
  • 0 kudos