Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S UART Receive problem

Posted on August 02, 2016 at 13:24I have a weird condition in which the STM8S003 does not read the entire packet I'm sending using a PC serial port. For example I have sent 256 bytes using a PC software but at the end I have only read 214 bytes inst...

GNNS1A1 Serial Issues.

Hi,I am currently attempting to create a development board stack up starting with a Nucleo-f401re, GNSS1A1, IKS01A2, and SX1276MB1LAS LoRa shield in the order listed. I was having difficulties getting two stack ups to communicate through radio and r...

GRaym by Associate
  • 746 Views
  • 0 replies
  • 0 kudos

Receiving Galileo frames ?

HelloAll examples available in CubeMX reguarding GNSS1A1 shield are using GPGGA frames, which, if I am right, are emitted by GPS satellites.I am interested with GAGGA frames from Galileo satellites, which are supposed to give better accuracy. Can yo...

YMARI by Associate
  • 866 Views
  • 0 replies
  • 0 kudos

Multisense timing diagram for VN7140ASTR-E-SO8

Hello Team,In the datasheet of VN7140ASTR-E ,the multisense timing diagram is available for Power SSO-16 in page number 19(figure 7),I want the multisense timing diagram for SO-8,Please provide the multisense timing diagram for SO-8 in current sense ...

ASrin by Associate
  • 826 Views
  • 0 replies
  • 0 kudos

what's the application scenario of the CPUDIV in CLK?

We can get the information that the CPUDIV can be used to divide fMATESR for CPU. And the divide ration can up to 128:1. I wonder that when you configure CPUDIV to 128:1, can CPU works normally when access peripherals such as I2C. Or CPUDIV is just ...

l yk by Associate II
  • 956 Views
  • 0 replies
  • 0 kudos

Hello, I am trying to initialize I2C, but getting continuously high signal on both SDA and SCL pins . Can anyone suggest what can be the issue?

#include "stm8s.h"#define I2C_PORT   (GPIOB)#define SDA_pin   (GPIO_PIN_5)#define SCL_pin   (GPIO_PIN_4)#define SLAVE_ADDRESS 0x60#define I2C_OWN_ADDRESS 0x00static void CLK_Config(void);void I2C_init(void);void I2C_Write(uint8_t I2C_Slave_Address,ui...

HJada by Associate
  • 2118 Views
  • 3 replies
  • 0 kudos