Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I'm using EEPROM M95080. It is mentioned that the IC will send data at the falling edge. But its not happening exactly at the falling edge(there is a delay of almost 0.2 microseconds after the falling edge).

1)The IC supports both the modes of SPI(CPOL =1,CPHA =1 and CPOL =0,CPHA =0). On the master side I have configured the SPI with CPOL = 1and CPHA = 1.2) According to this master SPI mode the master will receive data at the rising edge and the slave se...

PTiwa by Associate II
  • 2426 Views
  • 2 replies
  • 1 kudos

How to read the data from M95256 EEPROM?

I'm using M95256 IC which is used as an external EEPROM for the controller. When i'm sending Read Status Register command i can see data from IC in receive buffer. But when i'm sending Read from Memory command, i get only 0xFF data in the buffer.I ha...

ATUND by Associate II
  • 3092 Views
  • 3 replies
  • 0 kudos

Serial Issues

Hi, I am currently attempting to create a development board stack up starting with a Nucleo-f401re, GNSS1A1, IKS01A2, and SX1276MB1LAS LoRa shield in the order listed. I was having difficulties getting two stack ups to communicate through radio and r...

GRaym by Associate
  • 1034 Views
  • 0 replies
  • 1 kudos

STI7105KUDT/B32

May I know if it is a valid part number? I haven't find anything about B32.I have pictures on hand. Can you check if they are genuine ST parts?​

JDong.4 by Associate
  • 2404 Views
  • 3 replies
  • 0 kudos