cancel
Showing results for 
Search instead for 
Did you mean: 

How to read the data from M95256 EEPROM?

ATUND
Associate II

I'm using M95256 IC which is used as an external EEPROM for the controller. When i'm sending Read Status Register command i can see data from IC in receive buffer. But when i'm sending Read from Memory command, i get only 0xFF data in the buffer.I have checked the Status register after Write to memory command and the WIP = 0 and WEL=1 in the register. I'm not able to see the data on the oscilloscope as well even though i can see Read from memory command is getting transmitted in Tx Buffer as well as i can see it on oscilloscope.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Pierre P.
ST Employee

​Hello,

Please follow section 6.5 of datasheet attached.

Warning: Read operation can't be performed if a Write cycle is currently in progress.

Moreover, your status register value should be with WIP & WEL=0. I f WEL= 1 it means the write instruction didn't success.

0xFF correspond to the delivery state.

BR

EEPROM suPPort team

ATUND
Associate II

Hi,

My instructions sequence is:

1.WRITE ENABLE

2.WRITE STATUS REGISTER

3.WRITE DISABLE

4.READ STATUS REGISTER

5.WRITE ENABLE

6.WRITE MEMORY ARRAY

7.WRITE DISABLE

8.READ STATUS REGISTER

9.READ FROM MEMORY ARRAY

I have added delay of 5ms in between the instructions. But still the value of status register remains same i.e. WIP=0 and WEL=1.

Hi,

My instructions sequence is:

1.WRITE ENABLE

2.WRITE STATUS REGISTER

3.WRITE DISABLE

4.READ STATUS REGISTER

5.WRITE ENABLE

6.WRITE MEMORY ARRAY

7.WRITE DISABLE

8.READ STATUS REGISTER

9.READ FROM MEMORY ARRAY

I have added delay of 5ms in between the instructions. But still the value of status register remains same i.e. WIP=0 and WEL=1.