Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Greetings Friends,I have STM8S Discovery Board with STM8S105 micro controller. I want to use SWIM pin as general purpose IO and also want to use it to upload the code. Is there any possibilities ?
Hi all. I'm about to start a project where we just measure the voltage and current of a single phase 220V 50Hz line. We need all the usual values (P, Q, S, cos phi, etc) using a CT and a standard transformer for the voltage. We also don't care that m...
Hi sir,As per our application, we need to enable and disable the power supply IC enable pin. So we are using Flip flop based toggle function. so we are connect 12V rail directly (before voltage regulator).So as per ISO standard, our application shou...
It seems that the reference SPBT2632C2A.AT2 (Bluetooth V3.0, Class2) is unavailable.Therefore, we would like to know about a available compatible reference, both hardware and firmware.Could you help me with this issue?
I am facing some issue.I have described some steps below,please go through it and let me how can I fix this issue through Software?Is there any flag need to clear/set or anything?I am using TJA1028 LIN transreceiver for this.Monitor LIN bus and +5VCo...
Hi,I am working with the STM8AF5286UDY and am trying to set up a CAN interface.For programming, I use the standard peripheral library. At the moment, my CAN interface works fine. The only thing, which does not work, is the filtering.I use extended ID...