please tell me the programming Software used For ST10F276 controller
which software used to upload ST10F276 controllerST10 Flasher 2.2 or ST10 Flasher 2.4B tool?Please guide me
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
which software used to upload ST10F276 controllerST10 Flasher 2.2 or ST10 Flasher 2.4B tool?Please guide me
hello siri use the i2c bus on a stm8s208.there is just connected 2 pcf8574.the crystal i used is 8Mhz, and a i2c clock divider of 4one pcf8574 is connected to dipswitched , adress is 42the second pcf8574 is connected to led's, adress is 40individualy...
I am working with VND5T016ASP-E high side driver. By looking at the datasheet in current sense section, it says Vsense is tested at Iout =20A with Rsense =3.9kohm. by calculation I am not getting anywhere closer to 5V which is given as min value but ...
I would like to receive a string through the UART1, its format is from 000000000 to 999999999, However when I send the string only the first object is read and it is repeated nine times and the other values are lost.I am using this function to read t...
Hi. I'm using a STM8AF6226TDSSS chip. I can't find the specific model number on the website.STVP set STM8AF6226TxSSS as a different device apart from STM8AF6226. So what's the difference? Is the datasheet applicable?
I am using a stm8s103f which has 8K flash. My project compiles fine using the cosmic compiler. I get a map that looks like this .start 00008080 end 00008080 length 0 segment .const start 000080a1 end 00008924 length 2179 segment .text start 00...
Working way: W and Hold is high, Other SPI BUS.First we send "RDSR" Command but MISO is low like no working, so I try send "WREN" and "WRSR"but is no working.
Dring this time, will there by any electrical flow in other pins like SDI/SDO. If there is electrical flow, then I am interested to know how big it is ?