Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Device: STV5730A. I'm looking for inventory on the STV5730A. I'm finding inventory on the STV5730A1 or STV5730A-1. The data sheet does not mention an A1 or A-1 version.

Does anyone know the difference between the standard STV5730A, and the STV5730A1 or STV5730A-1 that I'm finding on the open market? The suppliers confirm that they are ST product. I can find the Data Sheet for the STV5730A, but no reference to an A...

I think there is a bug in the STM32CubeIDE Version: 1.4.0 Build: 7511_20200720_0928 (UTC), section “device configuration tool�?, section STMicroelectronics.X-CUBE-TOUCHGFX.4.15.0 Mode and configuration.

When Graphics Application is checked, a folders tree starting from TouchGFX, with files like GFX2.touchgfx, etc, is generated. It’s OK.When the .ioc file becomes complicated (as the example I attach), it seems that TouchGFX is replaced by Src and all...

AGendrau by Associate
  • 1065 Views
  • 1 replies
  • 0 kudos

STM8S003F3 - flash endurance and lab classes

Hello,The STM8S003F3 is a Value Line device with quite small number of write/erase cycles. The data sheet says:Program memory: 8 Kbyte Flash memory; data retention 20 years at 55 °C after 100 cycles---My wife is going to use very cheap W1209 thermost...

Is it possible to damage a STBP120 device by attached a low impedance voltage source set to 26V instantly to the input pin?

I have found when tapping a powered bench DC supply at 26V to the input pin of this OVP protection device, I seem to have destroyed the device. I measure 2.5 ohms from the input pin to ground and I measure 140 ohms between the input and output pins.

ADobb.1 by Associate
  • 590 Views
  • 0 replies
  • 0 kudos