Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
We are currently using the Ublox M8 receiver and are in the process of qualifying the Teseo-LIV3 as a possible replacement. One issue I'm having is the need to up the baud rate after initially connecting and configuring the receiver. The Ublox M8 d...
The only place I see future leap seconds mentioned, in the software manual, is in the GLONASS almanac message:KP Notification on forthcoming leap second correction of UTCAs I mentioned above, I would rather not have to request and then parse this alm...
For example the status of "STM8L15x/16x/05x/AL3Lx/AL31x standard peripheral library" STSW-STM8016 claims it is active. But the release notes seem to suggest that the last time someone took a look at it was at the end of 2014. That's not very active...
Hello everyone, I am using stm8l151, STVD, and cosmic compiler. I have multiple problems with STVD_STM8. Please help me as these are really confusing. I list some of them below:After I comment a line in the code, it is still active and the program st...
Hello ST Team,I'm doing interface between STM32F413 & ESP32 WROOM 32, but not getting how many pins of ESP32 WROOM 32 are going to use for interface with STM32F413.I'll going to do UART communication.How many program pins , data pins & control pins ...
It is fitted in a Bosch / Mopar Airbag Sensor ECU in a Jeep Renegade. Part number: 52042475 Airbag ECUI need to buy them to have some spare parts if I need, regards, Kleber
Hi, while the software are working, suddenly it will become stop, and reset pin is permanently forced low, it freaks me out!! Someone will help me, thank you so mutch
Hi,I need to modify data on a car's Lin bus line without generating errors on car side.I have two board with stm8 and can bus.my idea is to interrupt the car's lin bus line and connect my boards. but I don't know how to do it without affect the bus
Hello Everyone,I am using a STM8S105C6T6 in one of my application and I am facing problem while programming it.Software used: STVD version 4.3.12Compiler: Cosmic CXSTM8 Special Edition 4.5.1 (Free 1yr License version)I have build my application and w...