Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

delay_ms(1); missing prototype STM8S001J3

I code in STVD + COSMIC for STM8S001J3, it was prompted:----------- Project test_stm8s001j3 - STM8 Cosmic - Configuration Debug -------------   Compiling main.c... cxstm8 -if:\stm8\stm8s_stdperiph_lib\libraries\stm8s_stdperiph_driver -if:\stm8\stm8s_...

MQi.1 by Senior II
  • 1448 Views
  • 1 replies
  • 0 kudos

enable/diasble read-out protection (ROP)?

Hi,for a product I want to activate read-out-protection (ROP) via option byte, to prevent misuse via the SWIM interface. However, is it possible to disable it again from the application (given a "secret" condition)? Page 50 in RM0016 indicates that A...

GIcki by Associate II
  • 4563 Views
  • 4 replies
  • 0 kudos

How can I increase the amplitude of the sine wave generated from the pwm of the stm8s003f3 microcontroller ?? Is there any particular formula to calculate that??

I have a haptic button where the vibration has been set as soon as the pwm is genereated, I want to increase the vibration by changing the amplitude of the sine wave generated from the pwm, Can I know how can I do that??

SANAN.1 by Associate II
  • 3420 Views
  • 5 replies
  • 0 kudos

I'm using RH-PMICL1AK1 which is Engineering model of RHRPMICL1AK01V , its datasheet If the voltage drop on RSENSE exceeds 100 mV, the device enters the current limitation mode.However,actually only the voltage drop on RSENSE exceeds 125 mV.

hello,everyone:I'm using RH-PMICL1AK1 which is Engineering model of RHRPMICL1AK01V , its datasheet If the voltage drop on RSENSE exceeds 100 mV, the device enters the current limitation mode.However,actually only the voltage drop on RSENSE exceeds 12...

Dzefa.1 by Associate
  • 1014 Views
  • 0 replies
  • 0 kudos