Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STML432 unable to use both SPI modules in Mbed OS?

Hi there, I'm trying to interface with two different slave devices using the two SPI modules on the STML432kc with Mbed OS. Individually they work fine but as soon as i have both defined in the same program i run into hard faults. ​I'm aware of the p...

GRing.1 by Associate II
  • 797 Views
  • 0 replies
  • 0 kudos

Resolved! Unable to write to TIM2 Registers

I have this little project for the STM8L101F3 that just writes an arbitrary value to TIM2_CCR1H and TIM2_CCR1L and then tries to start the timer but I get nothing from the timer output.If I run the project with a debugger and inspect the contents of ...

AMacd.1 by Senior
  • 2802 Views
  • 8 replies
  • 0 kudos

Resolved! Can you help me identify this component?

Hi everyone!I'm new here and wasn't sure where to post so I apologize if this is in the wrong area.I've attached a picture of a component I'm in need of, but can't find it anywhere online. Can you please help me identify it?It's on a fog machine that...

CShar.3 by Associate II
  • 1969 Views
  • 3 replies
  • 0 kudos