Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Where do I get "STM8S standard firmware library"?

The "STM8S standard firmware library" is referenced in UM0834 for STM8S-Discovery. The library examples were well organized according to the descrription and included everything for the quick start. There were timers examples, ADC, SPI, I2C, UART exa...

SVino.4 by Associate II
  • 3016 Views
  • 3 replies
  • 0 kudos

In stm8s0003f3 ,I am reading analog voltage.I am getting the value in watch as 1544,which is not expected .Can some one help what may be the fault in the code. supply vge is 1.8v

void Init_ADC(void) {    ADC1_DeInit(); ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_5, ADC1_PRESSEL_FCPU_D2,         ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL5,DISABLE);  }void ADC_Read(unsigned int MV) { ADC1_...

SRAM.11 by Associate III
  • 1327 Views
  • 2 replies
  • 0 kudos