marking code
I have an SMD component, with the marking code WBCBR and it's a MOSFET, but I can't find the data sheet, can you help me?
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
I have an SMD component, with the marking code WBCBR and it's a MOSFET, but I can't find the data sheet, can you help me?
I'm looking for a replacement for a transistor. Naming on the transistor isST MRC BULK128DB W7R426I think it's discontinued. It's in a starter for fluorescent lighting which is probably around 12 years old.Any help would be greatly appreciated!
There is now a Release Candidate 1 for the 4.3.0 release of the Small Device C Compiler (SDCC), a free ISO C compiler targeting the STM8 and other 8-bit architectures.Source, documentation and binary packages for amd64 Windows, amd64 macOS and amd64 ...
Hi, I have two pin connection questions, related to EMIF03-SIM02M8: 1) Are VDD pins 1 & 8 connected internal to the chip or should be connected together externally?2) Pin 9, GND does it have to be connected to system ground, or that's optional?Any la...
I'm looking at this ST Micro part ST MICROELECTRONICS TSX339IQ4 --- power from 2.7V to 16V. But Vicm limitation of Vcc - 2V. At 3.3V-2V = 1.3V. But need Vcm at 2.5V., so 2.5V + 2V = 4.5V, so likely Vcc = 5V.as an alternative source...
Hi, I am trying to build 9 dof imu using LSM6DSO and LIS3MDL, using i2c to write and read lsm6dso and lis3mdl. I am testing the ICs in Raspberry Pi MCU. I am also using sensor hub on LSM6DSO to read/write LIS3MDL.I have two questions that I need help...
Hi, I'm designing a low power tilt and shake detection sensor module using the STM32 blue pill board. I'm trying my best to attain the datasheet values of 2-5µA. I have done the following:1) Set all GPIO pins to Analog 2) Disabled all peripherals man...
I am trying to confirm the marking ID on the physical part (4FFT 8311) UFDFPN-8 EP for St. Micro # M24C64-FMC6TG
Facing a challenge in implementing IoT-connected art in my gallery. The idea of sensors embedded in artworks communicating with each other or a central system sounds amazing, but I'm encountering some hurdles. Has anyone successfully tackled similar ...
Hello,So it seems like the software package X-CUBE-LED12A1, which is essentially a basic C driver for (some) of the dev kits, contains no support for uploading, downloading, starting or stopping execution of scripts. The commands are present in bridg...