Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Identify TPM serial number

Greetings and happy new year, ST folks, hope this message finds you well! I've got a ST33HTPHAHD8 and am hoping to track down its serial number.  Some documentation I've read suggests it might be available by way of an NV index or in the EK certifica...

aoswald by Associate
  • 2611 Views
  • 0 replies
  • 0 kudos

STM8L151K4 - Startup issues on external power

Hi,I'm having some issues getting code to actually run on the mcu. The power on reset doesn't appear to work, and I have to trigger an external reset via tying the NRST pin low to get the program to run. Cosmic + STVD was used, and STVP was used for ...

plebbbb by Associate
  • 1159 Views
  • 0 replies
  • 0 kudos

Resolved! L6262 2.6 Troubleshooting

Hello, I apologize if this is completely the wrong place to ask this question.  I've been trying to learn and soak up as much information as I can about PCB board design, components, etc through a restoration project on a very old hard drive.  But I ...

chip.png

IBIS model for IDPROM M24C02-F

I simulated the SDA with IBIS model downloaded, but I realize there is mismatch comparing the result to the datasheet. It's stated with Cload 10pF, the tF SDA falling time is minimum 20ns and max 300ns.With the ibis model, the same Cload, the falling...

QuestionFish_0-1704281186840.png QuestionFish_1-1704281393165.png

MEMS Board and accelerometer

I have finally isolated an example of the error. The MKI 210 accelerometer + the test board is sitting attached to a NUC computer.  The entire setup has run for months with no problems at a REMOTE LOCATION that is very hard to get to without a lot of...

Screenshot 2024-01-01 121541.png