cancel
Showing results for 
Search instead for 
Did you mean: 

edesign does not fit with input specifications

Gaston
Senior

Here's what eDesignSuite shows for a Boost DC/DC converter. The L7981 is a Buck converter so I don't understand the given results. Please anyone could clarify this?

Gaston_0-1698915085697.png

 

gaston

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

I am very sorry that the eDesign Suite displays this in a somewhat ambiguous way. STMicroelectronics does not have a boost regulator that can generate 24V from 13...18V without a circuit extension.

The L7981A is indeed a buck regulator, but like the other regulators shown (e.g. L7986A) it can be extended to a positive buck-boost with an external MOSFET. Such a regulator can then produce an output voltage that lies between the minimum and maximum input voltage, here e.g. 24V from 13...27V.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

I am very sorry that the eDesign Suite displays this in a somewhat ambiguous way. STMicroelectronics does not have a boost regulator that can generate 24V from 13...18V without a circuit extension.

The L7981A is indeed a buck regulator, but like the other regulators shown (e.g. L7986A) it can be extended to a positive buck-boost with an external MOSFET. Such a regulator can then produce an output voltage that lies between the minimum and maximum input voltage, here e.g. 24V from 13...27V.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.