cancel
Showing results for 
Search instead for 
Did you mean: 

Intelligent power module

safia-bashir
Associate

*Is it possible to utilize just one phase from the SLLIMM high-power IPM, which is a 3-phase inverter with a 650V short-circuit rugged IGBT rated at 50A? Additionally, do you have an IPM comparable to the discontinued STGIPS40W60L1, a half-bridge IGBT intelligent power module rated at 600V, 40A?"

0 REPLIES 0